C-Bus Module for Linux
                       Version 3.15

Welcome and thank you for installing C-Bus Module for Linux.

This software is used to develop interfaces to C-Bus, for Linux/x86 platforms.

The following components have been installed:

/usr/local/doc/cbus            - documentation
/usr/local/include/cbus	       - C header files
/usr/local/lib	               - Compiled library, used for linking to
                                 your application
/usr/local/src/cbus            - Source for the linux com port driver
/usr/local/share/cbus/examples - Sample programs for the command
                                 line and for GNOME / GTK+

The C-Bus Module is copyright (c) 2005 Clipsal Integrated Systems Pty Ltd.

Happy developing!


Release Notes.

Version 3.15 Defect defect corrections for HVAC to the interface guide
             document. Add APIs for clock & burden control. Add API for
             getting serial number as a string. Add API for setting the
             ramp to 0 mode.

Version 3.14 Minor defect corrections for HVAC. Make heating a valid
             lighting-like application.

Version 3.13 Updated air conditioning application API's to match update
             to protocol definition - sensor status now added.

Version 3.12 Updated air conditioning application API's to match update
             to protocol definition.
             Allow opening com ports > COM9 in Windows.
             Change ping counts so update rates < 100ms don't ping PCI
             too often.
             Prevent the transmit queue process from doing anything if
             in transparent mode.

Version 3.11 Windows-only defect - not released for Linux.

Version 3.10 Fixed a defect that caused buffer overflow when transmitting
             very long labels. Updated Windows and Linux open of serial
             port to set modem control signals to allow use of C-Touch
             as a PCI.

Version 3.9 Fixed a defect that caused loss of some traffic transmitted
            to C-Bus under conditions of sustained extremely high load.

Version 3.8 Updated HVAC TYPES to a new and more complete set.
            Increase the number of lighting applications from 10 to 20.

Version 3.7 HVAC Set Plant Level changed to signed.
            Added latched_shortcut to error application API's.

Version 3.6 Add event handlers for change of preferred language

Version 3.5 Add ability to detect and report that the PCI has been
            disconnected. See section 10.2.6 of the Interface Guide.

Version 3.4 Ensures the C-Bus PCI is restored to a default state when the
            serial port is closed.

Version 3.3 Adds support for the C-Bus Error and Air-Conditioning Applications.