C-Bus Module for Linux
                       Version 3.2

Welcome and thank you for installing C-Bus Module for Linux.

This software is used to develop interfaces to C-Bus, for Linux/x86 platforms.

The following components have been installed:

/usr/local/doc/cbus            - documentation
/usr/local/include/cbus	       - C header files
/usr/local/lib	               - Compiled library, used for linking to
                                 your application
/usr/local/src/cbus            - Source for the linux com port driver
/usr/local/share/cbus/examples - Sample programs for the command
                                 line and for GNOME / GTK+

The C-Bus Module is copyright (c) 2005 Clipsal Integrated Systems Pty Ltd.

Happy developing!