C-Bus Module for Linux
                       Version 3.5

Welcome and thank you for installing C-Bus Module for Linux.

This software is used to develop interfaces to C-Bus, for Linux/x86 platforms.

The following components have been installed:

/usr/local/doc/cbus            - documentation
/usr/local/include/cbus	       - C header files
/usr/local/lib	               - Compiled library, used for linking to
                                 your application
/usr/local/src/cbus            - Source for the linux com port driver
/usr/local/share/cbus/examples - Sample programs for the command
                                 line and for GNOME / GTK+

The C-Bus Module is copyright (c) 2005 Clipsal Integrated Systems Pty Ltd.

Happy developing!


Release Notes.

Version 3.5 Add ability to detect and report that the PCI has been
            disconnected. See section 10.2.6 of the Interface Guide.


Version 3.4 Ensures the C-Bus PCI is restored to a default state when the
            serial port is closed.

Version 3.3 Adds support for the C-Bus Error and Air-Conditioning Applications.